april 12, 2022
Award-winning System
Murrelektronik's VARIO-X automation system wins two awards, the international prize for "Best equipment, best system for the factory of the future" and the Computer & Automation Audience Award, within a few days.

Twin pack for Murrelektronik! The company has won two prestigious awards - the "Factory of the Future" award in the category "Best Equipment, Best System", presented at the "Advanced Factories Congress" in Barcelona and the Audience Award for Product of the Year in the "Communication & Networking" category, presented by "Computer & Automation" magazine - with its brand new "VARIO-X" automation system. Both awards recognize Murrelektronik's outstanding future viability and innovative strengths.
VARIO-X is a modular, highly flexible automation system that, for the first time, allows all automation functions to be decentrally (without control cabinet architecture) implemented. It brings sensors and actuators into the direct machine environment and ensures reliable voltage, signal and data management during the seamless integration of decentralized servo drives. The accompanying digital twin saves time and money during planning, installation, operation and service. "We are delighted to receive these two awards. They are confirmation of our efforts to constantly question automation and drive it forward with new approaches and ideas. That's why they are not only confirmation for us, but also an incentive to continue on our chosen path to decentralized digitalization with all the consistency we can muster," Christian Kübler, VARIO-X product manager at Murrelektronik, is pleased to report.
För nedladdning
Senaste nytt från vårt företag
Vario-X: The days of the control cabinet are numbered
Murrelektronik is expanding its business model and, with Vario-X, offers the first completely decentralized automation platform that brings devices into the field without control…
Xelity 10 TX IP67: A switch for every application
The Xelity 10 TX IP67 managed switch from Murrelektronik offers new possibilities for decentralized, cabinet free, data management. With up to ten Gigabit ports in a robust…
Multitalented Masters
Murrelektronik expands its IO-Link portfolio with the IP67 rated MVK Pro and IMPACT67 Pro fieldbus modules. The robust modules provide on-board diagnostics and 4A per port output…